Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Electrical Distribution

News: Electrical Distribution

The TeSys F AC3 range of contactors is the smart choice for demanding motor applications

   


15/03/2016
- The TeSys™ F AC3 range of contactors offers a wider scope of current and control voltage ratings to satisfy requirements for building, industry, and data centre environments. This includes demanding applications such as HVAC, hoisting, and more.

  • Optimised size for reduced panel space
  • High reliability, safety, and durability
  • Type 1 & 2 coordination with Compact & Masterpact™ circuit breakers
  • Shared accessories with entire TeSys F range
  • Drawer-mounted coils allow easy maintenance
  • Operating range up to 1000 A and 670 kW, at 440 VAC

Get world-class quality and a robust design that makes installation, maintenance, and upgrading easy

> Discover the TeSys F AC3 range