|
|
The construction business today is all about finding robust, safe and strong building materials that are cost-effective and easy to handle. Hollow core slabs are one of the most frequently used types of pre-fabricated concrete floors in office buildings today. Now it is possible to take advantage of this hidden capacity underneath the floor level.
Schneider Electric is the first manufacturer to launch a floor box system that is tailor-made for hollow flooring with cavities of Ø 170 mm or larger. With the OptiLine Hollow Core Box together with OptiLine 45 or 50 floor boxes, you can install electricity and cabling without affecting the floor strength. Power and data will be easily accessed, offering significant benefits for the installer as well as for the end-user.
|
To reduce the overall building height, the demand for lower floor boxes has increased, resulting in less coupling space. But with the Hollow Core Box from Schneider Electric, no extra floor height is required and there is plenty of room for connections and cable loops as well as for bulky transformers. Still, the floor box lid can be closed.
 |
|
Hollow core box with OptiLine 50 floor box in stainless steel |
 |
|
OptiLine 50 and 45 Hollow core box for hollow core slabs |
To know more about OptiLine Hollow Core Floor Box
Brochure
> OptiLine 45 Hollow core floor box
> OptiLine 50 Hollow core floor box
Video
> OptiLine 45 Hollow core floor box
> OptiLine 50 Hollow core floor box