With over 70 years' expertise, Schneider Electric proposes hoisting control solutions which can save up to 30% in handling time. They enhance reliability, safety, performance of your cranes. The drive controller includes ready-to-use and efficient dedicated hoisting functions (anti-crab, anti-sway, smooth slewing functions…). They allow preventive maintenance through real time tracking of component usage. Reduce maintenance thanks to an immediate incident register which enables you to quickly diagnose problems, prevent component failure and anticipate the need for possible replacement components.