|
 |
Gaining time in all of a project’s development and installation phases is vital if installation commissioning dates are to be met.
|
 |
 |
Go for simplicity
- Measure, manage, analyse and diagnose all the applications in an installation.
- A comprehensive range with a relay that corresponds exactly to your requirements.
- Designed for the following applications:
- substation, - transformer, - generator, - capacitor bank, - busbar, - motor.
- Management of the functions needed for each application (protection, measurement, control, temperature, etc.)
|
|
|
 |
|
 |
Modular construction |
 |
Configure it with peace of mind |
 |
Communicate: be open |
|
|
|
|
|
|
 |
|
| |
|
| |
190
Schneider Electric has a presence in 190 countries
48 h
Sepam availability throughout the world
A requirement for quality
- Design based on operating dependability studies.
- Design meets IEC 61508 functional safety requirements.
- ISO9001 certified development and production.
- Manufacturing methods that respect the environment (ISO14001).
|
|
|