Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Contractors
                                                   
                                                 
                                                 

                                                Back to Panelbuilders home

                                                 
                                                   
                                                 
                                                 
                                                 

                                                Lighting control

                                                Achieve simple lighting control using natural light and building occupation

                                                 
                                                 

                                                Main drivers:

                                                “I want to reduce the amount of energy used by my building’s lighting by taking advantage of natural light in corridors and areas with large windows. Most importantly, I want to keep lights from being left on all weekend!”

                                                Solution in brief:

                                                Solution applicable to any building without a Building Management System and with good natural light

                                                A controller is programmed with each area’s occupation patterns. A light sensor allows the lights to be switched on, via the controller, when natural light levels are too low. The system is flexible enough to allow occupants to override the restriction, switching lights on for short periods of time as needed.

                                                Each area is outfitted with the usual light fixtures and push-button on/off switches, and is powered by an electrical circuit controlled by an impulse relay that receives commands from a controller. The controller also includes digital inputs from one or more twilight switches that constantly measure natural light levels.

                                                Depending on the configuration, the controller can either automatically switch lights on in a given area, depending on time of day, or periodically send lights-off commands when natural light is high, or when the programmed occupation time is over. Flexible programming ensures an optimal balance between energy savings and user comfort.

                                                Benefits for End Users:

                                                > Save 10% off lighting costs, one of the top three sources of electrical consumption
                                                > Easy-to-control, independent system does not affect other building systems

                                                Benefits for professionals:

                                                + Design

                                                • Fully-configurable for a variety of building occupation situations

                                                 

                                                + Installation

                                                • Offer the added value of automation
                                                • Impulse relays work with standard wiring

                                                 

                                                + Maintenance

                                                • Easy-to-maintain traditional architecture

                                                Architecture:

                                                 

                                                Around the world
                                                  
                                                 
                                                To know more

                                                To know more 

                                                Requests for Solutions, Products and Services information

                                                Customer care center operator on the phone
                                                 

                                                Application to achieve simple lighting control

                                                 

                                                Main products