Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Contractors
                                                     
                                                   
                                                   

                                                  Back to Panelbuilders home

                                                   
                                                     
                                                   
                                                   
                                                   

                                                  Energy monitoring

                                                  Get essential electrical information for each area of your building

                                                   
                                                   

                                                  Main drivers:

                                                  “As facility management contractor, I need a system that can gather, track, and clearly display electrical information for different areas of my building.”

                                                  Solution in brief:

                                                  Install meters to send information to a PC equipped with PowerView consumption-tracking software

                                                  PowerView software is one of the easiest ways to improve a building’s energy efficiency. It is also the perfect foundation for upgrading to more sophisticated systems later on.
                                                  The easy-to-use interface displays measurements and the associated curves in real time. Both PM9c and more advanced PM710 meters use a RS485 Modbus protocol. An EGX100 gateway converts Modbus into Ethernet TCP IP protocol

                                                  Benefits for End Users:

                                                  > Savings of up to 10% with ROI within the first year
                                                  > Individual metering raises occupants’ awareness of consumption
                                                  • Power is switched off immediately to unoccupied areas to keep consumption on track
                                                  • Power factor is adjusted to ensure optimal efficiency and reduce power-factorrelated penalties

                                                  Benefits for professionals:

                                                  + Installation
                                                  • Available as a power-meters-plussoftware bundle
                                                  • PowerView software is easy to use
                                                  • PM9c, PM710 and EGX100 meters suitable for LV switchboard installation
                                                  • DIN-rail-mounted PM9c and EGX100 suitable for renovation projects
                                                  • PM710 meters same size as old analog ammeters or voltmeters for door mounting
                                                  • Factory-calibrated PM9c meters leave just a few settings to be selected on site
                                                  + Maintenance
                                                  • Automatic identification of any new Schneider Electric meter installed, for fast and easy upgrades

                                                  Architecture:

                                                  ENEGRY_MONITORING_Get_essential_energy 

                                                  Around the world
                                                    
                                                   
                                                  To know more

                                                  To know more 

                                                  Requests for Solutions, Products and Services information

                                                   

                                                  Application to get essential electrical information for each area of your building

                                                   

                                                  Main products