Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Contractors
                                                   
                                                 
                                                 

                                                Back to Panelbuilders home

                                                 
                                                   
                                                 
                                                 
                                                 

                                                HVAC control- Regulate cooling-tower water temperature and save energy

                                                 
                                                 

                                                Main drivers

                                                “My cooling tower is a constant concern. Maintenance needs vary widely depending on the season, and the installation uses too much energy. I want a solution that will improve yield and reduce costs.”

                                                Solution in brief

                                                Use speed drives to regulate the tower’s fan and pump

                                                Solution applicable to medium-sized to large buildings with cooling tower

                                                The best way to control air-water exchange in a cooling tower is to use variable speed drives to control  the tower’s fan and pump, eliminating additional maintenance-hungry mechanical systems while  meeting the tower’s needs. A PLC regulates fan airflow and pump volume via the variable speed drives.

                                                This solution uses up to 50% less energy than direct-start fans and pumps and eases maintenance. Over a given season, the fan and pump motors must operate at full speed just 2% to 5% of the time—the rest of the time this energy is wasted. Direct-start motors require additional mechanical systems to solve problems like fan blade rotation due to wind, or additional resistance due to freezing.

                                                This solution uses 20% less energy than two-speed motors and also improves maintenance. While two-speed motors offer a partial solution to energy consumption issues, they do nothing to resolve maintenance issues.

                                                Benefits for End Users

                                                > Reduce energy consumption
                                                > Improve yield by regulating water temperature
                                                > Lower maintenance requirements, especially in extreme weather
                                                > Quieter operation
                                                > Low harmonics: THDI < 30%
                                                > Eliminates inrush current due to motor start-up

                                                Benefits for professionals

                                                + Simpler mechanics (no brakes, sensors, or rotation inverters)
                                                + Facilitates motor sizing (over-speed and standby modes available)
                                                + Enhanced process regulation
                                                + Extends lifetime of mechanical components
                                                + Facilitates maintenance planning

                                                Architecture

                                                  

                                                  
                                                 
                                                To know more

                                                To know more 

                                                Requests for Solutions, Products and Services information

                                                Customer care center operator on the phone
                                                 

                                                Speed drive application in cooling tower

                                                 

                                                Main products HVAC Control