Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image


Contractors


                                                   
                                                 
                                                 

                                                Back to Panelbuilders home

                                                 
                                                   
                                                 
                                                 
                                                 

                                                Building management

                                                Monitor and control electrical loads in your retail shopfront

                                                 
                                                 

                                                Main drivers

                                                “I need to be able to check the status of the oven, refrigerator and security cameras quickly and easily when I close up my shop. I want to make sure everything is secure and avoid wasting energy.”

                                                Solution in brief

                                                Install KNX current sensing switch actuators connected to a touch panel to monitor loads

                                                 

                                                Solution applicable to all commercial buildings; particularly suitable for retail

                                                The touch panel shows the status of the different loads and indicates potential risks—such as the refrigerator, oven, or security system—during shop opening hours.

                                                The system cuts power to specific loads—like an oven left on at night—thus eliminating waste. It also helps to ensure proper operation of the security system by monitoring devices like security cameras and lighting.

                                                A KNX logic module rotates the lighting sources used at night from one night to the next for more even use of light fixtures. The touch panel provides information on the operating hours and expected lifetime of  each fixture, for more efficient maintenance and replacement.

                                                Benefits for End Users

                                                > Monitoring consumption and identifying unnecessary use can generate savings of up to 10% and more
                                                > Lower maintenance costs by rotating lighting sources
                                                > Reduce energy consumption
                                                > Increase safety of people and property through automatic alarms and emergency calls
                                                > Added convenience of remote monitoring and control
                                                > Easy upgrades and extensions

                                                Benefits for professionals

                                                + KNX systems are easier to design than traditional systems with similar functions
                                                + Requires working with a skilled electrician or planner/ integrator to get maximum user-friendliness and cost-effectiveness
                                                + Maximum flexibility, making adjustments to layout much easier than with traditional systems

                                                Architecture

                                                 

                                                Around the world
                                                  
                                                 
                                                To know more

                                                To know more 

                                                Requests for Solutions, Products and Services information

                                                Customer care center operator on the phone
                                                 

                                                Application to monitor and control electrical loads in your retail shopfront

                                                Monitor and control electrical loads in your retail shopfront
                                                 

                                                Main products