Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Contractors
                                                   
                                                 
                                                 

                                                Back to Panelbuilders home

                                                 
                                                   
                                                 
                                                 
                                                 

                                                Power distribution

                                                Reduce power loss by filtering harmonics

                                                 
                                                 

                                                Main Drivers

                                                “I need to reduce the overall harmonics generated by my factory’s variable speed drives and uninterruptible power supply. My budget is limited, and the solution has to be simple.”

                                                Solution in brief

                                                Install AccuSine PCS active filtering for your electrical installation

                                                Solution applicable to small to medium-sized buildings

                                                Variable speed drives and uninterruptible power supplies constitute non-linear loads. They use a fundamental sine wave (the same frequency as the network) and generate additional harmonics
                                                waves whose frequencies are multiples of the network’s frequency.
                                                The AccuSine PCS active filter constantly generates an equal yet opposite current to the harmonic currents generated by non-linear loads, leaving only the fundamental frequency on the network.
                                                The AccuSine PCS is fed from a specific outgoing feeder. It detects and analyzes the current upline in real time from the non-linear loads and sends out a compensating current via its power line.
                                                The following oscillograms illustrate the total current harmonic distortion (THDI) before and after the installation of the act

                                                 

                                                Benefits for End Users

                                                > Harmonic filtering reduces power loss in the upline circuit and equipment by 10%
                                                > Ensures harmonics of less than 5%
                                                > Reduces overloading and frees up additional useable capacity
                                                > Minimizes system losses and demand power
                                                > Lowers outage risk
                                                > Extends equipment lifetime
                                                > Reduces wire heating (especially neutral)

                                                Benefits for professionals

                                                + Easy to install
                                                + Compensation automatically adjusted depending on load
                                                + Easy upgrades and add-ons
                                                + Optional power factor correction possible (recommended by utilities)

                                                Architecture

                                                 

                                                Around the world
                                                  
                                                 
                                                To know more

                                                To know more 

                                                Requests for Solutions, Products and Services information

                                                Customer care center operator on the phone
                                                 

                                                Application to reduce power loss by filtering harmonics

                                                reduce power loss by filtering harmonics