Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Contractors
                                                     
                                                   
                                                   

                                                  Back to Panelbuilders home

                                                   
                                                     
                                                   
                                                   
                                                   

                                                  Renewable Power Generation

                                                  Supply a small group of remote, off-grid buildings with electricity

                                                   
                                                   

                                                  Main drivers

                                                  “We would like to provide electricity to a remote village in Africa. We are looking for the optimized technical solution at the best price.”

                                                  Solution in brief

                                                  Install solar panels to provide the buildings with their own independent energy supply

                                                   

                                                  Solution applicable to off-grid buildings

                                                  The system includes:

                                                  • Solar panels with a total capacity of a few kWc
                                                  • 1 Xantrex XW solar charge controller
                                                  • A set of batteries to store several days’ worth of electricity
                                                  • 1 Xantrex Trace TR1524 inverter
                                                  • Circuit breakers to protect the solar installation and for each building
                                                  • 1 GSM-equipped iRio unit for remote management of network operating schedule and monitoring of consumption, batteries, the charger, the solar panels, and the inverter
                                                  • urge protection devices for PC photovoltaic generators and for the AC part of the installation

                                                  Benefits for End Users

                                                  > Totally independent electricity supply
                                                  > Local, independent management of the installation

                                                  Benefits for professionals

                                                  + A single interface for centralized management and monitoring
                                                  + Local people receive maintenance and operation training from Schneider Electric

                                                  Projects

                                                  Madagascar village gets solar energy In early 2009, solar panels were installed in a mountain village in Madagascar. The village, which counts about 20 houses, was too remote to be connected up to the
                                                  main grid. The goal was to provide 50 W for each household three hours per day— a total of 1,000 W for the village or 3 kWh per day.
                                                  According to a survey conducted after the project was completed, the local population, which helped with the work, was satisfied with the results. A team of two local electricians received training from Schneider Electric Madagascar. They did the wiring in all of the houses and now handle maintenance and repairs.

                                                  Architecture

                                                   

                                                    
                                                   
                                                  To know more

                                                  To know more 

                                                  Requests for Solutions, Products and Services information

                                                   

                                                  Application to supply a small group of remote, off-grid buildings with electricity

                                                  Supply a small group of remote, off-grid buildings with electricity
                                                   

                                                  Main products