Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Contractors
                                                     
                                                   
                                                   

                                                  Back to Panelbuilders home

                                                   
                                                     
                                                   
                                                   
                                                   

                                                  Renewable Power Generation

                                                  Use available rooftop space to install and operate solar panels

                                                   
                                                   

                                                  Main drivers

                                                  “I want green certification for my farm. I would like to install rooftop solar panels on one of my outbuildings, but only if it is profitable for the business.”

                                                  Solution in brief

                                                  Convert the energy generated by solar panels into alternating current and connect to the three-phase grid

                                                  Solution applicable to commercial and farm buildings with roof surfaces < 500 square meters

                                                  The system consists of photovoltaic panels that produce between 30 kW and 50 kW of electricity by transforming solar energy into direct electric current. This “convert, connect, protect” system is built around prefabricated, interconnected panels:

                                                  • Panel strings are interconnected via junction boxes to pool the electricity generated by the photovoltaic installation
                                                  • An inverter then converts the direct current produced by the panel strings into alternating current
                                                  • Factory-assembled, pre-wired protection units ensure the installation is safe for both people and property.

                                                  Benefits for End Users

                                                  > Helps businesses qualify for green certification
                                                  > ROI of less than 10 years driven by selling surplus power back to the grid (in countries where incentives are offered)
                                                  > Clear information thanks to SunEzy inverters, which monitor both the electricity used and old back to the grid
                                                  > Easy to upgrade to a building management system without changing the installation

                                                  Benefits for professionals

                                                  + Schneider Electric support to help you choose the right solution
                                                  + All products, including panels, cables, and inverters, provided by a single Schneider lectric-approved
                                                  distributor
                                                  + Add on to the installation without making costly changes
                                                  + Meets environmental standards

                                                  Architecture

                                                   

                                                    
                                                   
                                                  To know more

                                                  To know more 

                                                  Requests for Solutions, Products and Services information

                                                  Customer Care Center
                                                   

                                                  Application to use available rooftop space to install and operate solar panels

                                                  Use available rooftop space to install and operate solar panels