Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Contractors
                                                     
                                                   
                                                   

                                                  Back to Panelbuilders home

                                                   
                                                     
                                                   
                                                   
                                                   

                                                  Energy Monitoring

                                                  View and monitor the energy used by your lighting installation

                                                   
                                                   

                                                  Main drivers

                                                  “I want to get an overview of the different loads in my retail space so that I can identify areas for potential savings.”

                                                  Solution in brief

                                                  Install a KNX system to meter and monitor the different loads in your building

                                                   

                                                  Solution applicable to small retail buildings 

                                                   

                                                   The solution is based on EN40p electric meters at the electrical distribution level.
                                                  For each KWh used, a given number of pulses are sent from the meter to the KNX binary input.
                                                  Consumption data is then transferred to the 10” IP touch panel, where it can be viewed and processed.

                                                  The touch panel can also be used to view and control current building states and functions.

                                                   

                                                   

                                                  Benefits for End Users

                                                  > Reduce energy consumption by up to 10% and more: monitoring energy use enables you to identify waste and encourage more energy-efficient behaviour
                                                  > Increase safety by automating alarms and emergency calls
                                                  > Enjoy the convenience of remote monitoring and control
                                                  > Lower installation costs than traditional systems with similar functions

                                                  Benefits for professionals

                                                  + Flexible, for easy add-ons and modifications: all equipment is connected via a common bus line allowing you to reconfigure or expand the installation without costly building work
                                                  + New opportunities for your business: KNX solutions must be implemented by skilled electricians
                                                  or integrators and offer an array of user-friendly, cost-effective functions

                                                   

                                                  Architecture

                                                  View and monitor the energy used by your lighting installation 

                                                    
                                                   
                                                  To know more

                                                  To know more 

                                                  Requests for Solutions, Products and Services information

                                                   

                                                  Application to view and monitor the energy used by your lighting installation

                                                  View and monitor the energy used by your lighting installation
                                                   

                                                  Main products