Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Contractors
                                                     
                                                   
                                                   

                                                  Back to Panelbuilders home

                                                   
                                                     
                                                   
                                                   
                                                   

                                                  How to choose the correct surge protection regarding a situation?

                                                   
                                                   

                                                  Which type of surge arrester for which situation?

                                                  Types of surge arresters

                                                  • T1: only used when LPS is present
                                                  • T2: used systematically.
                                                  • T3: only used in addition to a T2 (as lower discharge capacity), if the loads are more than 30m from the incoming T2 surge arrester

                                                  * LPS (Lightning Protection System) = lightning rod, meshed cage on buildings)
                                                  ** After 30m (between the surge arrester and the loads) lightning wave reflection phenomena appear in the cables.

                                                  The 30 meters rule for installation of surge protection devices

                                                  Around the world
                                                    
                                                   
                                                  To know more

                                                  To know more 

                                                  Surge protection guide:

                                                   

                                                  Understand how to choose an upstream protection