Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Contractors
                                                     
                                                   
                                                   

                                                  Back to Panelbuilders home

                                                   
                                                     
                                                   
                                                   
                                                   

                                                  Select the right upstream protection for a surge arrester

                                                   
                                                   

                                                  The surge arrester has the same lifetime as the switchboard

                                                  At the end of its life, a thermal protector integrated into the surge arrester isolates the surge arrester from the rest of the installation.
                                                  It activates the red end-of-life warning light, indicating that the surge arrester needs to be changed.

                                                   

                                                  The role of the surge arrester is to drive the lightning current to the earth in a  very short time (< 350 microseconds).

                                                  However, the surge arrester is not intended to be exposed to a permanent overvoltage (phase/neutral inversion, or neutral rupture). In this case, it would be short-circuited and may damage the switchboard.

                                                   

                                                  A device protecting the surge arrester against short circuits is therefore required to ensure the safety of the electrical installation.

                                                   

                                                  When making the choice of an upstream protection device,

                                                  Take into account:

                                                   
                                                  • lightning current withstand capacity (to avoid nuisance trpping),
                                                  • short-circuit withstand capacity of the installation (Isc).

                                                  E.g. the best disconnection circuit breaker for a breaking capacity of 15kA and Imax of 40kA is a C60H.

                                                   Newt page: Install an overvoltage protection 

                                                  Around the world
                                                    
                                                   
                                                  To know more

                                                  To know more 

                                                  Surge protection guide:

                                                   

                                                  Learn how to install surge protection