Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
 

                           
                           
                           

                          Intersolar Europe 2011

                          June 8-10, 2011 – Hall B4 booth 270 New Munich Trade Fair Centre Munich – Germany

                           
                           

                          Schneider Electric exhibited at this years Intersolar Europe 2011 tradeshow that took place in Munich from June 8-10, 2011. 
                          Don’t miss out on our Video that sumarizes Schneider Electric’s participation at the Tradeshow!


                          This image can't be displayed
                          Get Adobe Flash player
                           
                           
                           
                           
                           

                          Schneider Electric products and solutions featured at Intersolar Europe 2011 included single-phase and three-phase inverters, a full-solution PV Box, an innovative new charge controller, and highly evolved monitoring solutions:

                          • Conext™ Series Grid Tie Solar Inverters, which are designed to offer improved reliability and a low installed cost through ease of installation and integrated features.
                          • XC Series Central Inverters, a new line of central inverters designed for high efficiency and flexibility for any PV panel type and installation.
                          • PV Box, a complete solution including power conversion, electrical distribution, control, monitoring, and communication designed to meet the growing demand of a large-scale grid-tied solar farms and large commercial installations in any region of the world, even in the harshest environments.
                          • Xantrex™ XW MPPT 80 600 Solar Charge Controller, an innovative solar charge controller that accepts PV array voltages up to 600VDC, significantly simplifying system installation and reducing size and cost for array wiring and associated hardware.
                          • Monitoring Solutions provide harmonized communication through two dedicated monitoring systems, one for buildings and power plants and one for residential and commercial applications, with data accessible from anywhere, anytime through the web.
                               
                             
                           

                          Free Solar Power Solutions Guide

                           

                          > Download the Power Solutions Guide

                           
                             
                            
                           
                          To know more

                          To know more 

                          Intersolar

                           

                          Renewable energies