Today, 20% to 40% of the poorest populations revenue is dedicated to getting an energy that is often harmful for the environment, for health, and not reliable. With In-Diya, Schneider Electric offers an innovative, affordable and flexible solution to bring reliable, efficient and green lighting to people living without access to electricity . In-Diya is a LED based lighting system that can operate on power from grid and / or solar panel and / or battery for indoor applications, adapting to the different conditions of the people.
* BoP : Base of the Pyramid