The Altivar 11 range is replaced by the Altivar 12 range.
Variable speed drives for small machines with three-phase 240 V asynchronous motor
0.18 to 0.75 kW, 120 V single-phase power supply
0.18 to 2.2 kW, 240 V single-phase power supply
0.18 to 4 kW, 240 V three-phase power supply
- Can be configured in its packaging
- Quick start option requiring no adjustment
- Intuitive navigation
- Even more compact
- Category 1 EMC filter
- Local control on the front panel
- Modbus serial link
- Resistant to harsh operating environments