Enclosed DOL starters are used to control starting and stopping of the machine
TeSys motor-starter solutions incorporate 2 auxiliary contacts which allow them to be integrated in safety wiring diagrams
TeSys Vario switch disconnectors
Installed on an enclosure or in a cabinet, these rotary control switch disconnectors act as circuit load breakers
Available in open or enclosed version
Fixed on the front panel or DIN rail mounted
Padlockable versions
Thermal-magnetic motor circuit breakers TeSys GV2-ME
Vario switch disconnector
TeSys GV2-ME motor circuit breaker
More foresight for better prevention
A range of safety control products which are simple to use and set up, with compact ergonomic products to meet requirements for starting and stopping motors.
All machines requiring:
DOL starting and stopping of motors
load breaking of the machine control circuit