Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Electrical Distribution

News: Electrical Distribution

Schedule selected loads simply via your BMS (Building Management System)

Integrate a centrally- managed load- shedding system into your BMS (Building Management System). The solution is built around a PC or PLC that controls load shedding. The controller is used to generate load shedding orders based on the electrical variables of the entire electrical installation, taking into account time bands, operating, or even process-related information.
This solution to integrate a centrally- managed load- shedding system into your BMS reduces up to 10% electricity bills.


This solution is part of a set of Building management solutions. In this chapter, you will discover how our building management system delivers capabilities like complex data analysis and detailed consumption trend reporting while integrating consumption and installation control features.


You can find more energy efficiency solutions for buildings in a 35-solutions catalogue with Schneider Electric products.

> Register to receive the complete pdf catalogue of 35 solutions for energy efficiency in buildings.