Electrical Distribution
News: Electrical DistributionRegulate temperature by maintaining air pressure using variable speed driveUse variable speed drives to regulate air pressure and temperature. Take a chilled-beam heating system, for example. The most energy- efficient solution for this type of heating system would be to add temperature regulation functions via a thermostat, plus pressure regulation in the beam and the room.
This solution is part of a set of HVAC control application sheets. In this chapter, you will see how HVAC energy consumption levels can be reduced by improving the control and management of ventilation, temperatures, and system usage, with speed drive and motor starter.
> Register to receive the complete pdf catalogue of 35 solutions for energy efficiency in buildings.
|