Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Electrical Distribution

News: Electrical Distribution

Achieve simple lighting control with natural light and building occupation

In this application, you need first to program a controller with each area’s occupation patterns. Via the controller, the light sensor allows the lights to be switched on when natural light levels are too low. The system is flexible to allow occupants to override the restriction, if required.
With this application coordinated of controller and light sensors, you can save 10% off lighting costs.

 

This solution is part of a set of Lighting control solutions. In this chapter, you will see how to slash your lighting costs by 50% compared to traditional systems.

 


You can find more energy efficiency solutions for buildings in a 35-solutions catalogue with Schneider Electric products.

 

> Register to receive the complete pdf catalogue of 35 solutions for energy efficiency in buildings.