Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
 
 
 
 

Power control contactors

 
 
TeSys Contactors mini modular and variable composition contactors 

TeSys Contactors
The world leading TeSys family of contactors has a huge variety of mini modular and variable composition contactors suitable for almost every conceivable motor switching or distribution circuit switching application.

Contactors

> Contactors 0,06 kW to 5,5 kW TeSys K
> Contactors 0,06 kW to 75 kW TeSys D
> Contactors 55 kW to 450 kW TeSys F
> Bar Contactors up to 900 kW TeSys B