Products and Services
Optional Device Drivers for ION EnterpriseOptional device drivers add support for device types that are not included with your version of ION Enterprise by default. They are provided as self-installing executables, which makes it easy to add additional device support to your ION Enterprise system. There are two kinds of device drivers for ION Enterprise:
Standard Edition (SE) Device Drivers SE device drivers provide support for real-time registers, onboard data logs (including events, data and waveforms), control functions (including resets, triggers and digital outputs) and they come with a complete set of Vista diagrams. These drivers are only compatible with ION Enterprise 6.0 Service Pack1. Please ensure that your ION Enterprise system has the latest Service Pack applied before installing an Optional Device Driver.
LE device drivers provide support for real-time registers only. They come with a complete set of Vista diagrams. Some LE drivers will include pre-defined PC-based logging for mapped registers. Please refer to the "Translator Details" document for information about which measurements are mapped and which ones are captured in PC-based logs. LE device drivers do NOT extract any data from logs onboard the device (events, alarms, interval data or waveforms). LE device drivers do NOT support control actions (such as triggering or control of digital outputs / relays). LE device drivers do NOT support setup registers for device configuration. LE device drivers are NOT editable using the Modbus Device Importer (MDI) LE device drivers are only compatible with ION Enterprise 5.6 Service Pack 2 (SP2) or ION Enterprise 6.0 Service Pack 1 (SP1) systems. Please ensure that your ION Enterprise system has the latest Service Pack applied before installing an Optional Device Driver.
|