Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Installation Systems & Control
     
     
     

    KNX system

    KNX actuators

     
     
    KNX consists of a twin-core bus line and bus-compatible installation devices such as sensors, actuators and system components, that are connected to it.

    Actuators receive data telegrams and convert these e.g. into switching or dimming signals. Actuators are selected depending on the required application and consist of a bus coupler and an application module with the corresponding application program. The application programs are part of the Schneider Electric product database.

    They are loaded into the devices together with the project design and commissioning software ETS via the serial interface of a PC and the bus.

       
    This image can't be displayed
    This image can't be displayed