Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Installation Systems & Control
     
     
     

    KNX system

    Blind and switch actuators

     
     

    The blind/switch actuators are especially practical, and available for 8-blind/16-switch setups or for 12-blind/24-switch setups.

    Each channel can be operated either as a blind channel or as a switching channel. In the "Switching" channel operating mode, one blind channel is divided into two equal switching channels. The channels must be toggled at the device itself and in the ETS.

    It is not possible to invert the blind and switching channels. If the software and hardware configurations of the parameterized channels are not aligned, the relays of the affected channels are immediately opened and disabled.

       
     
     
     
     
     

    Available products

    KNX bli.act. REG-K/4x/6

    Bli.act. REG-K/4x/24V w.man.mode

    KNX rol.shut.act.REG-K/4x/10 w.man.mode

    KNX bli.act.REG-K/2x/10 w.man.mode

    KNX bli.act.REG-K/4x/10 w.man.mode

    KNX bli.act.REG-K/8x/10 w.man.mode

    KNX bl.sw.act.REG-K/8x/16/10 w.man.mode

    KNX bl.sw.act.REG-K/12x/24x/10 w.man.mo

    Weather combi sen. / DCF77 bk

    Weather station REG-K/4-gang lgr

    MTN646704

    MTN648704

    MTN649704

    MTN649802

    MTN649804

    MTN649808

    MTN649908

    MTN649912

    MTN663692

    MTN682991

    This image can't be displayed
    This image can't be displayed