Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Installation Systems & Control
     
     
     

    KNX system

    Dimming actuators

     
     

    Schneider Electric offers different devices for dimming, such as a dim actuator, four universal dim actuators, 2 x 1-10 V control units and 2 x DALI gateways.

    The universal dimmers for series installation, with their energy-saving technology, adapt automatically to every load type and are an ideal solution.

       
     
     
     
     
     

    Available products

    KNX dim act REG-K/2x230/300W

    KNX Uni.dim.act.REG-K/230/1000W

    KNX Uni.dim.act.REG-K/230/500W

    KNX Uni.dim.act.REG-K/2x230/300W

    KNX Uni.dim.act.REG-K/4x230/150W

    KNX Cont.un. 0-10V REG-K/3g w. man.mode

    KNX Cont.un. 0-10V REG-K/1g w. man.mode

    KNX DALI-Gateway REG-K/1/16/64

    KNX DALI-Gateway REG-K/1/16(64)/64

    KNX Uni. dim. act. REG-K/4x230/250W

    MTN646630

    MTN649310

    MTN649350

    MTN649330

    MTN649315

    MTN646991

    MTN647091

    MTN680129

    MTN680191

    MTN649325

    This image can't be displayed
    This image can't be displayed