Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Installation Systems & Control
     
     
     

    KNX system

    KNX Logic module

     
     

    Combining different building functions makes many aspects of daily life easier, whether in the office or at home. The new logic module Basic REG-K is a perfect supplement to KNX applications – an optimal logic operation and controlling building functions are made simply possible.

    Intelligent control – KNX Logic module Basic REG-K
    Thanks to the logic module, special logic operations can be initiated between actuators and sensors creating numerous logic functions for controlled KNX devices. This added value in comfort, security and savings in energy and costs is made possible by the numerous functions that the logic module offers.

    The KNX Logic module Basic REG-K offers comfort
    Flexible conference rooms with movable walls need a flexible connection between push buttons and switch/dim or blind actuators. That is a typical application for logic module’s multiplexer function.

    The KNX Logic module Basic REG-K offers security
    Do you want to make sure that you closed all the windows when you left the house? This is easy with the logic module. With this device, all the window contacts are linked and the status of the windows can be clearly shown, for example, on an info display in the corridor.

    The KNX Logic module Basic REG-K saves energy, time and money
    Supermarkets, for example, do not switch off their lights completely at night. Thanks to the logic module, the lights age at the same rate because a different row of lights is switched on every night. This rotating system saves the service technician time and the operator saves money.

     
     
     
     
     

    Available products:

    KNX Logic module REG-K

     

    MTN676090

     

    This image can't be displayed
    This image can't be displayed