Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Installation Systems & Control
     
     
     

    KNX system

    Switch actuators

     
     

    The Schneider Electric actuators fulfill all your customers' wishes. Schneider Electric has the right switch actuators for every application, which distinguish themselves by their simple installation.

    The switch actuators are available as 2-gang, 4-gang, 8-gang and 12-gang version. Whether it be small or large loads, no problem!

    The switch actuators are available from 6 A to 16 A with electrical or mechanic manual mode.
    Furthermore, selected actuators have current detection, which detects the load current of each channel, an operating hours counter, a switch-on counter and an integrated power meter.

       
     
     
     
     
     

    Available products

    KNX sw.act. REG-K/8x230/6

    KNX sw.act. REG-K/2x/10 w.man.mode

    KNX sw.act.REG-K/4x/10 w.man.mode

    KNX sw.act.REG-K/8x/10 w.man.mode

    KNX sw.act.REG-K/12x/10 w.man.mode

    KNX sw.act.REG-K/2X230/16 w.man.mode

    KNX sw.act.REG-K/4X230/16 w.man.mode

    KNX sw.act.REG-K/8x230/16 w.man.mode

    KNX sw.act.REG-K/12x230/16 w.man.mode

    KNX switch act.REG-K 2g w.curr.detec.

    KNX switch act.REG-K 4g w.curr.detec.

    KNX switch act.REG-K 8g w.curr.detec.

    KNX switch act.REG-K 12 g w.curr.detec.

    KNX sw.act.FM/230/16

    MTN646808

    MTN649202

    MTN649204

    MTN649208

    MTN649212

    MTN647393

    MTN647593

    MTN647893

    MTN648493

    MTN647395

    MTN647595

    MTN647895

    MTN648495

    MTN629993

    This image can't be displayed
    This image can't be displayed