Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Installation Systems & Control
     
     
     

    KNX system

    KNX sensors

     
     

    KNX consists of a twin-core bus line and bus-compatible installation devices such as sensors, actuators and system components, that are connected to it.

    Sensors record information that is transmitted to the bus in the form of a data telegram. Sensors are e.g. KNX pushbuttons and binary inputs for connecting floating contacts.

    Sensors are selected depending on the required application.

    The application program is loaded into the devices together with the project design and commissioning software ETS via the USB interface of a PC and the bus.

       
    This image can't be displayed
    This image can't be displayed