Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Installation Systems & Control
     
     
     

    KNX system

    Movement / presence detectors

     
     

    Schneider Electric KNX movement detectors - a smart solution.
    Can be connected directly to the KNX bus. Thus several movement detectors can be integrated into a network using a KNX bus. This ensures safety all through the building.

    Switching, dimming and blind functions can for instance be triggered easily and conveniently using the three different movement detector outputs.
    Any movements detected are communicated discreetly to an information display in the form of text messages, and can be read there.

    Schneider Electric KNX presence detectors are used to integrate the demand-dependent control system into the building management system. This also makes available other options for intelligent and economical operation.

    The optional light control makes the most of the possibilities and ensures a high degree of comfort with reduced energy costs for the system.

       
         
     
     
     
     
     

    Available products

    KNX ARG Presence 180/2,2m FM TPb pw SysM

    KNX ARG Presence 180/2,2m FM TPb aw SysM

    KNX ARG Presence 180/2,2 FM TPm ant SysM

    KNX ARG Presence 180/2,2 FM TPm alu SysM

    KNX ARG Presence Basic pw

    KNX ARG Presence Basic alu

    KNX ARG Presence pw

    KNX ARG Presence alu

    KNX ARG Presence w. light cont.+IR pw

    KNX ARG Presence w. light cont.+IR alu

    KNX ARG 180 FM TPb pw SysM

    KNX ARG 180 FM TPb aw SysM

    KNX ARG 180 FM TPb w SysM

    KNX ARG 180/2,2m FM TPb pw SysM

    KNX ARG 180/2,2m FM TPb aw SysM

    KNX ARG 180/2,2m FM TPb w SysM

    KNX ARG 180 FM pw SysD

    KNX ARG 180 FM w SysD

    KNX ARG 180 FM stst SysD

    KNX ARG 180 FM alu SysD

    KNX ARG 180 FM TPm ant SysM

    KNX ARG 180 FM TPm pw SysM

    KNX ARG 180 FM TPm w SysM

    KNX ARG 180 FM TPm alu SysM

    KNX ARG 180/2,2m FM TPm ant SysM

    KNX ARG 180/2,2m FM TPm pw SysM

    KNX ARG 180/2,2m FM TPm w SysM

    KNX ARG 180/2,2m FM TPm alu SysM

    MTN630419

    MTN630425

    MTN630614

    MTN630660

    MTN630719

    MTN630760

    MTN630819

    MTN630860

    MTN630919

    MTN630960

    MTN631619

    MTN631625

    MTN631644

    MTN631719

    MTN631725

    MTN631744

    MTN631819

    MTN631844

    MTN631846

    MTN631860

    MTN632614

    MTN632619

    MTN632644

    MTN632660

    MTN632714

    MTN632719

    MTN632744

    MTN632760


     

    This image can't be displayed
    This image can't be displayed
    This image can't be displayed