Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Installation Systems & Control
     
     
     

    KNX system

    KNX system components

     
     

    KNX comprises a two-wire bus line and the connected bus-compatible installation devices, such as sensors, actuators and system components.

    System devices and components are required for the fundamental system functions. These are essentially power supplies for generating the bus voltage, couplers for connecting bus section.

     
    This image can't be displayed
    This image can't be displayed