Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Installation Systems & Control
     
     
     

    KNX system

    IP-Router

     
     
    The KNX/IP router enables telegrams to be forwarded between different lines via LAN (IP) as a rapid backbone.

    The device can additionally serve as a programming interface in order to connect a PC with the KNX bus (e.g. for ETS programming with suitable ETS). The IP address can be assigned dynamically via a DHCP server or via manual configuration (ETS parameter).

    The device operates in accordance with the KNXnet / IP specification using Core, device management, tunnelling and routing.
    The KNX/IP router forwards telegrams in both directions whilst taking a filter table into account and can buffer up to 150 telegrams.
       
     
     
     
     
     

    Available products

    Coupler REG-K

    KNX IP-Router REG-K

    MTN680204

    MTN680329

    This image can't be displayed
    This image can't be displayed