Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Electrical Installation Guide
Download the electrical installation guide
 
 
 

The Electrical Installation Guide 2015 is now available

 
 
   

What’s new in the 2015 edition ?

  • Updated list of relevant IEC standards.
    For example, the new standard IEC60364-8-1 “Low-voltage electrical installations - Part 8-1: Energy efficiency” published in October 2014
  • New content about LED lighting: characteristics and particular constraints of LED luminaires, selection tables to choose the proper circuit-breakers and relays
  • New content about Arc Fault Detection Devices (AFDD), as defined by new IEC 62606 (2013) and updated IEC60364-4-42 (November 2014)
  • “Connection to the MV utility distribution network” chapter completely re-written and updated, with more detailed information about protection in electrical installations, including the introduction of service continuity classes.
  • “MV and LV architecture selection guide for buildings” chapter partly re-written and including a description of the barycentre method, recommended by the new IEC 60364-8-1, to select the optimal location for the transformers and switchboards
  • New content about the selection of busways (busbar trunking systems) in presence of harmonics
  • Updated Energy Management architectures
   

Table of contents

Table of contents

  • General rules of electrical installation design
  • Connection to the MV utility distribution network
  • Connection to the LV utility distribution network
  • MV and LV architecture selection guide for buildings
  • LV distribution
  • Protection against electric shocks and electric fires
  • Sizing and protection of conductors
  • LV switchgear: functions and selection
  • Overvoltage protection
  • Energy efficiency in electrical distribution
  • Power factor correction
  • Power harmonics management
  • Characteristics of particular sources and loads
  • PhotoVoltaic (PV) installation
  • Residential and other special locations
  • ElectroMagnetic Compatibility (EMC)

Download the electrical installation guide

             
   

A practical guide for the complete design of an electrical installation according to IEC 60364 and other relevant IEC standards

The Electrical Installation Guide has been written for electrical engineers who must design, select electrical equipment for, install this equipment into, inspect, or maintain low-voltage electrical installations in compliance with the standards published by the International Electrotechnical Commission (IEC). “Which technical solution will guarantee that all relevant safety rules are met?” Answering this question has always been integral to the creation of this document.

     

Covering many topics related to electrical installations

Such as voltage drop, electrical safety, cable sizing, electrical calculations, electrical standards, electrical design, electrical protection, circuit breakers, MV/LV substations, earthing schemes, electromagnetic compatibility, power factor correction, harmonics, overvoltage protection…

           
   

Written by Schneider Electric’s most talented electrical distribution experts

Sharing their latest state-of-the-art knowledge about new or updated electrical installation standards, technological evolutions…
The Electrical Installation Guide is also available in a Wiki format to let any and all experts contribute to its elaboration.

   

For anyone involved in commercial, industrial, or domestic electrical installations

All professionals including consulting engineers, designers, contractors, panel builders, facility managers, as well as electrical engineering students and teachers, and also people involved in standardization, certification, or inspection of these electrical installations.