Xantrex does not provide solar array design advice as the charge controller is a single component in a complicated and site dependent system. The webpage you are about to access (the “Xantrex Sizing Tool”) is intended only as a guide for Xantrex customers requesting assistance with array sizing. In no way is it intended to be a guarantee of the performance of Xantrex inverter products or array compatibility, and should not be relied on for solar array design advice for the reasons set out below. It is the responsibility of the user of the Xantrex Sizing Tool to confirm the correctness of the Reference inputs, the formulas behind the calculations and the output of the Xantrex Sizing Tool. Xantrex recommends that in the design of any system that a qualified installer be contacted to confirm the output of the Xantrex Sizing Tool and the correct solar array.
There are a number of factors that may affect the output of the Xantrex Sizing Tool or the appropriate use of a charge controller in an array design including, but not limited to, the following:
A Xantrex charge controller will (i) shut down when DC voltage exceeds its rated open circuit voltage (VOC), and if it does it will require a manual reset and may even be damaged; and (ii) may not be able to maximum power point track (MPPT) at voltages close to the battery voltage. Applications involving extreme temperatures or low fill factor modules often push the limits of this specified voltage range. This may mean that the controller only operates above the voltage at max power point on the hottest days. The Xantrex Sizing Tool is heavily dependent on the accuracy of the input data provided by the user and it does not account for module voltage degradation over time. Xantrex also relies on module specifications provided by the manufacturer of such module and can not guarantee the accuracy of such information.
THE USER OF THE XANTREX SIZING TOOL ACKNOWLEDGES that:
(i) The Xantrex Sizing Tool is being offered free of charge as a guide only and is not to be relied upon as solar array design advice,
(ii) the warranty for Xantrex products is governed by warranty terms contained in a separate Limited Warranty,
(iii) Xantrex makes no representation or warranty regarding the output of the Xantrex Sizing Tool, and
(iv) the user agrees to use the Xantrex Sizing Tool at its own risk and with the knowledge that Xantrex will not be liable to the user for any damages as a result of use of the Xantrex Sizing Tool.
YOUR USE OF THE XANTREX SIZING TOOL CONFIRMS YOUR AGREEMENT TO THE ABOVE: