Select a country
Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
International Customer Lounge (ICL) showroom - Paris
                     
                     
                     

                    The Square: an area dedicated to energy efficiency in buildings

                     
                     

                    Schneider Electric solutions provide customers with a global response to their energy efficiency requirements.


                    Discover The Square, area of the International Customer Lounge (ICL) of Schneider Electric  

                    The Square houses the HED (Hive Energy Display) and the NOC (Network Operating Centre).

                    The HED is the application/interface that places the spotlight on Building. Technical Management data and enables Schneider Electric to measure its real-time energy consumption.
                    It is both:
                    • an indicator of Schneider Electric headquarters energy consumption, and
                    • a tool which increases everyday awareness in energy savings

                    The NOC: “Network Operating Centre” is the place from which an entire communication network is supervised and controlled.
                    The NOC highlights the Schneider Electric product offer designed to supervise and control all types of sites, in order to optimise energy consumption, increase safety, control processes and render operators more efficient.
                    A number of scenarios are offered at the ICL (Building, Data Centre and Industry) based on the vision and mission of managers involved in each project type: building operators, safety managers, IT managers, etc.


                    > Discover the photo gallery area of the International Customer Lounge (ICL) showroom


                    > Back to the ICL showroom home page

                     

                    Register now and visit tomorrow the International Customer Lounge (ICL) of Schneider Electric
                      
                     
                    To know more

                    To know more 

                    • The ICL is able to welcome 
                      20 000 visitors a year

                    • The visit is conducted in 5 languages

                    • The visit lasts roughly 60 min

                    • The showroom surface area measures 1000 m²

                    • You will walk 300 m

                    • The visit is accessible to disabled persons