Making permanent savings through Active Energy Efficiency
Active Energy Efficiency is defined as effecting permanent change through measurement, monitoring, and control of energy usage. Passive Energy Efficiency is regarded as the installation of countermeasures against thermal losses, the use of low consumption equipment, and so forth.
It is vital, but insufficient, to make use of energy-saving equipment and devices such as low-energy lighting. Without proper control, these measures often merely militate against energy losses rather than make a real reduction in energy consumed and in the way it is used.
Everything that consumes power must be addressed actively if sustained gains are to be made. This includes changing the culture and mindsets of groups of individuals, resulting in behavioural shifts at work and at home, but clearly this need is reduced by greater use of technical controls.
To know more
Discover
Find out more
To read documents in Pdf format you need the plugin Acrobat Reader