Hospitals
Hospitals logo

Lighting Control

 

Pains & drivers

Lighting controls are a proven means to quickly lower energy costs. We integrate all control features associated with lighting including: occupancy detection, dimming, daylight linking, scene-setting and blind control, either from a centralised intelligent control panel or a distributed system. This can lead to a reduction in energy consumption of 25-50% in most spaces.
 

How can a customer manage energy more efficiently?

  • Lighting can represent up to 40% of energy consumption in buildings depending on segments.
  • Lighting control is definitely one of the easiest ways to save energy costs on one of the most common applications. Applying an effective lighting control solution, users can easily save up to 50% on their electricity bill compared to traditional ways.
 

Solutions or architectures used in the application

  • The solution provides automatic means to optimise lighting based on the 3 main parameters indicated above (time, intensity and presence), alone or combined.
  • The solution can range from very local and small solutions, such as timers, up to very sophisticated, customised but flexible, centralised solutions as part of building automation systems.
 
 
 
Schneider Electric Solutions
Schneider Electric SolutionsEase of InstallationEase of UsePotential SavingsIntegrated Supervisory Control


IC 100 + Cell, C60N

n/an/an/an/a


n/an/an/an/a
 
 
 

To know more 

Requests for Solutions information

Contact Customer Care Centre