Mining, Minerals, Metals
Mining, Minerals, Metals logo

Pump & Fan Control (Industry/Infrastructure)

Pains & drivers

  • In Industry, 70% of electrical consumption is used to turn motors. Of these motors, 33% control pump or fan applications.
  • Most pump and fan applications are driven by a SoftStarter DOL solution. This means that the motor runs at full speed and the flow variation is obtained. The energy consumption falls very little when the flow decreases. At 80% of the nominal flow, the energy consumption remains at 95%. The potential for saving on the installed base is huge.
  • The CEMEP association has carried out a simulation for the European market. The use of Drive in such applications could save 900 M Euro/year as well as 4 Million tons of CO2/year.
 

How can a customer manage energy more efficiently?

  • To save energy you must:
    - drive the motor with a frequency inverter instead of a contactor or Soft Start
    - remove the restriction device (valve or damper)
  • The AC Inverter allows you to adjust the speed of the Pump or the Fan, and therefore the Flow
  • The result is huge savings compared to conventional solutions:
    - up to 50% for a Fan, return on investment for the drive is within one year
    - up to 30 % for a Pump, return on investment within 2 years
 

Solutions or architectures used in the application

 
Solutions or architectures used in the application
A) Solution without Drive
The motor turns at a fixed speed according to the network frequency and the number of poles.
Example: 3600 Rpm for 60 Hz
2-pole motor
The only way to adjust the Flow is a restriction device (damper) which generates losses.







B) Energy Saving Solution with Drive
The Drive, which is also called a frequency inverter, lets you vary the frequency and therefore the motor speed, too.
The Flow is directly proportional to the speed.
The damper or valve are no longer required.







C) Energy Consumption with and without Drive
Example for Fan Application

Outlet damper
Variable speed drive
50% of energy saving at 80% of the nominal flow


Example for Pump Application

Control valve
Drive
30% of energy saving at 80% of the nominal flow 

 
 
 
Schneider Electric Solutions
Schneider Electric Solutions


Enhance safety,reliability while reducing operational costs with Integrated Oil & Gas Pipeline Management Solution combining Process, Energy & Security


Altivar 61





PlantStruxure

 
 
 

To know more 

Requests for Solutions information

Contact Customer Care Centre