Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image
Oil & Gas
            Oil & Gas logo

            Reference: Oil & Gas

            Total Indonesia (Indonesia)

            Renovation of the electrical equipment at the Senipah oil handling terminal in Kalimantan

            Reference: Oil & Gas
             

            I. CUSTOMER ENVIRONMENT / PROJECT CONTEXT

             

            Customer profile:

            Total is the leading French investor and the third overseas oil operator in Indonesia. Present since 1968, it holds 50% of the production-sharing contract for the Mahakam license signed with the national Indonesian company Pertamina, which groups several sites including Senipah.

             

            Customer objective and constraints:

            Renovate the electrical equipment at the Senipah site, located on the East coast of Kalimantan, in order to increase its operational service life by 10 years.

             

            II. SOLUTION IMPLEMENTATION

             

            Implementation methodology (main phases):

            Renovation was carried out without any modification to civil engineering or to switchboard MV/LV cable connections while also limiting downtime to the strict minimum.

             

            Duration:

            For Projects & Engineering Centre: 6 months

             

            Solution overview (services, products, systems, architectures...):

            As part of this project, Total Indonesia has entrusted Schneider Electric with the renovation of MV and LV equipment.

            Studies

            • Audit
            • Consultancy and expertise
            • Renovation
            • Diagnostic, measurement and monitoring

            Supply

            • 28 MV retrofits
            • 21 LV retrofits
            • 208 T12 drawers
            • Replacement of CEE relays by Sepam relays

            Commissioning

             

            III. RESULTS / ACHIEVEMENT

             

            Customer benefits:

            The substitution solutions limit investments and reduce maintenance costs. They are more economic than a new installation.

             

            Renovation was carried out without any modification of civil engineering or to switchboard MV/LV cable connections while also limiting downtime to the strict minimum.

             

            IV. ADDITIONAL INFORMATION

             

            Other information

            Following the creation of a new substation for the industrial gas treatment and compression site of Peciko in 1999, Schneider Electric has once again been contacted for renovation of the Senipah site.

             
             
             
             

            To know more 

            Requests for Solutions information

            Contact Customer Care Centre
             

            Solution breakdown

            Main services:
            • Engineering services: Services
            • ED audit consulting & Diagnostics MP4
            • Retrofit / retrofil
            • Refurbishment / revamping



            Replacement of 28 MV circuit-breakers installed in Belledonne cubicles:
            • retrofit of 1 DSE22 circuit-breaker by LF2 in B200,
            • retrofit of 5 DSE22G circuit-breakers by LF1 in B200G,
            • retrofit of 22 CD1 contactors by Rollarc R400D in P500D_



            Replacement of 21 LV circuit-breakers in T12 switchboard:
            • retrofit of 18 Selpact circuit-breakers by Masterpact NT,
            • retrofit of 3 Selpact circuit-breakers by Masterpact NW.



            R
            eplacement of 208 LV drawers in T12 switchboard:
            • 76 with contactors (65 drawers one module - 11 drawers two modules),
            • 132 with circuit-breakers (30 drawers two modules - 102 drawers one module).



            Replacement of CEE relays by Sepam relays.