Water logo

Water solution: Modular solution for pumping and additional treatment


Value proposition

Main drivers:
  • For booster or complex pumping stations.

Solution in brief:
  • Modular solution to manage more than 4 pumps and additional functions such as chlorination or tank management.

Value proposition:
  • Based on Altivar 61 drives, this solution allows you to reduce energy consumption by 20% to 30% on pumps depending on their characteristics. Energy savings are easily estimated via ECO8 software

Differenciation factors:
  • Flexible, this solution proposes high diagnostic capabilities thanks to Transparent Ready features and its connection to the Ethernet Network.



To know more 

Requests for Solutions information

Contact Customer Care Centre

Success Stories


Solution breakdown

Main products & systems: