Energy Efficiency

Automated lighting in foyer cloakroom

 
 

 

Value proposition

Solution in brief
  • A simple and efficient solution based on 360° movement detector easely installed on the ceiling of the entrance hall.

Value proposition

  • This solution provides a potential energy saving of 8% to 16%.
  • Automatic control of lighting according to brightness level. A switch (optional) hidden from users' view, allows ON override of lighting if required.

Differentiation factors

  • The absence of a light switch within reach of the public is more hygienic and ensures that the lighting is not switched on when it is not needed.
  • Aesthetically pleasing and discreet appearance that makes it appropriate for all types of premises.
 

Architecture

Architecture
 
 
 
 

To know more 

Requests for Solutions information

Contact Customer Care Centre
 

Key downloads

 

Solution breakdown

  • Main products & systems
   _ Movement detector: MG CDM 360
   _ Protection circuit-breaker: MG Multi9 C60
   _ Flush-mounted switch (optional)
   _ CT contactor and its associated circuit-breaker
      if power consumption exceeds 1 kW.