Energy Efficiency

Control office lighting locally

 
 

Value proposition

Main drivers

  • To optimise operating costs by saving lighting energy in the offices.

 

Value proposition

  • Up to 25% energy saving by automatically extinguishing lighting when it is not necessary.
  • Easy modification of the time switch programme for special events and holiday periods avoiding useless energy spending.

 

Differentiation factors

  • Using IHP+2c and TL to control office lighting locally by pushbuttons and centrally by a programmable time switch.
 

Architecture

 
Architecture

Control the lighting of the building:

  • By a centralised order transmitted by an impulse type IHP+ 2c to the ATLc+s impulse relay auxiliary.IHP+ 2c functions provide the benefit of centralised:

     - time programming,

     - manual override operation.

  • Locally by means of pushbuttons and benefit from TL functions:

     - blue remote control Off on the TL,

     - manual operation using the TL toggle.

 

Main Energy Efficiency characteristics

The solution is to control the lighting of the building:

  • by a centralized order transmitted by an impulse type IHP+ 2c to the ATLc+s impulse relay auxiliary

  The IHP+ 2c functions provide the benefit of centralised:

   time programming + manual override operation.

  • locally by means of push-buttons and benefit from TL functions:

   blue remote control OFF on the TL + manual operation using the TL toggle.

 
 
 
 

To know more 

Requests for Solutions information

Contact Customer Care Centre
 

Success Stories

 
 
 
 
 

Solution breakdown


Main products and systems:
  • Programmable time switch: IHP+2c
  • MCB 2 poles: C60N
  • Impulse switch: TL
  • Impulse relay: ATLc+s
  • NO push-button: PB (as wiring device is local, to be replaced by national one)