Energy Efficiency

Optimise room lighting through the use of dimmers

 
 

Value proposition

Main drivers

  • To reduce lighting-related energy consumption
  • To change room atmosphere 
  • To improve comfort

 

Value proposition

  • Up to 20% energy saving by dimming your light level by 25%
  • Wall box dimmers allow reduction of energy used for lighting
  • Instead of having lights only ON or OFF, light level can be adjusted to required level

 

Differentiation factors

Using a dimmer:

  • enables the homeowner to control light level independently 
  • allows to control light sources from one or several control points
 

Architecture

 

Solution breakdown & architecture are under validation: the content will probably move

Architecture
 

Main Energy Efficiency characteristics

Four Unica dimmer switches are available, according to the type of load to be controlled, the type of dimming (push button or rotary) and the possibility of associating them with other control devices.

Unica dimmer switches can:

  • save energy, since dimmed lighting uses less electricity than full power lighting
  • extend the lifetime of the light using the soft-on dimmer function
  • adapt the light level to fit the desired atmosphere in the room
  • regulate the lighting by simply pressing or rotating, according to the choice of product
  • be installed easily without changing the wiring.
 
 
 
 

To know more 

Requests for Solutions information

Contact Customer Care Centre
 

Solution breakdown


Main products and systems:
  • Pushbutton dimmer switch: Unica
  • MCB 1 pole: C60N
  • Pushbutton: PB