Energy Efficiency

Staircase & Corridors Lighting optimization through timers

 

Value proposition

Main drivers
  • Building managers need to increase user comfort and save on lighting-related energy spendings.

Solution in brief
This solution enables to set lighting times to a minimum in passageways thanks to a timer making it possible to:
  • Light one or several light sources from one or several control points,
  • Keep lighting on for a pre-set time,
  • Switch it off automatically.
  • Override the timer for permanent lighting when necessary.

Value proposition
  • Staircase timer allows reduction of energy spent for lighting. Instead of having the staircase and corridors permanently lit, the lighting is reduced to a pre-defined amount of time after one of the push-buttons connected to the timer is pressed.
  • Without this timer solution, the light is often on permanently. With the timer, energy spent can be reduced by to 30 to 50% .
 

Architecture

Architecture
 

Main Energy Efficiency characteristics


In addition to significant energy savings, Automation provides:
  • Greater comfort,
  • Better security.
  • Implementation is extremely simple.
  • An up to 7-minute time delay can be set.
  • The "override" function on the front face enables permanent lighting for cleaning and maintenance services.
 
 
 
 

To know more 

Requests for Solutions information

Contact Customer Care Centre
 

Solution breakdown

  • Main Products & Systems
    _
    MIN timer
    _ C60 type protection circuit-breaker.
    _ CT contactor and its protection circuit-breaker if the power consumed is above 2 kW.